An offset already exists on one or more of the selected faces.

2019-05-15T17:16:17Z

Summary


Details

When offsetting a face already used in an existing Offset Feature command, the 
following message is displayed: 
 An offset already exists on one or more of the selected faces. 
 Do you want to continue? 
 <<Yes>> <<No>>


How can this message be turned off?


Steps to reproduce the message: 
1. Select 'File-->New' and create a new part file. 
2. Select 'Insert-->Design Feature-->Cylinder'. 
3. Set options as desired and 'OK' the Cylinder dialog. 
4. Select 'Insert-->Offset/Scale-->Offset Face'. 
5. Select the cylindrical face as the 'Face to Offset'. 
6. Set any distance and 'OK' the Offset Face dialog. 
7. Select 'Insert-->Offset/Scale-->Offset Face'. 
8. Select the same cylindrical face as in step 5. 
9. Set any distance and 'OK' the Offset Face dialog. 
You will receive the above message.



Solution

 This message can be turned off by the following setting in Customer Defaults. 
1. Select 'File-->Utilities-->Customer Defaults'. 
2. Expand 'Modeling' and highlight 'General'. 
3. Select the 'Miscellaneous' tab. 
4. Toggle off 'Warn when Creating Offset on Offset'. 
5. OK the Customer Defaults dialog. 
6. Re-start NX for the setting to take effect.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V8.5
Function: FEATURE_MODEL

Ref: 001-6910877

KB Article ID# PL8010645

Contents

SummaryDetails

Associated Components