Create CGM from Modeling application with hidden edges removed in NX.
Solution
To remove the hidden edges so they do not display in a CGM:
1. Set the current display to "Static Wireframe".
This is the on screen method:

This is the icon method:

2. NX12 and earlier releases: 'Preferences -> Visualization -> Visual (tab) -> General Display Settings -> Part Settings (Selected Views) -> Rendering Style: Static wireframe -> Edge display settings -> Hidden Lines: Invisible.



NX1847 and later releases: 'Preferences -> Visualization -> Rendering -> Styles -> Render Style: Static Wireframe -> Static Hidden Edges: Invisible'.


Now create the CGM which will only export the displayed edges and not the hidden edges while in the Modeling application.
Notes and References
This shows how to export hidden line CGM's from both pre and post NX1847 as the preferences changed.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 10_1703
Product: NX
Application: GATEWAY
Version: V1847
Function: CGM_EXPORT
Ref: 001-6756779