Why is the 'Perimeter' dimension grayed out and unavailable?

2019-05-15T17:19:56Z

Summary


Details

In the cascading menus, select 'Insert-->Dimension' and notice that the 
'Perimeter' command is grayed out and unavailable. 
Why is the 'Perimeter' dimension grayed out in the Drafting application?



Solution

 The 'Perimeter' command becomes available when there is an active Sketch in 
the drawing. 
1. In the Part Navigator, highlight a view in a drawing sheet. 
2. 'MouseButton3-->Active Sketch View'. 
3. Select 'Insert-->Sketch Curve' and select a Sketch Curve command. 
The sketch will become active and the 'Perimeter' command will be available.


However, once 'Finish Sketch' is selected, the 'Perimeter' command will once 
again be grayed out.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V8.5
Function: DIMENSION

Ref: 001-7114905

KB Article ID# PL8010638

Contents

SummaryDetails

Associated Components