Automatic centerlines do not follow the customer default settings

2019-07-31T14:03:24Z

Summary


Details

Automatic centerlines generated when a drafting view is created, or by the Automatic Centerline command, do not use the values defined in Customer Defaults.


This can occur when the drawing is created within same part file as the model. 
The values being used are the customer default values when the model/part was first created, which may be different from the current values.



Solution

Use the command 'Tools --> Drafting Standard' to select and 'Apply' the required Drafting standard, before creating the view, to ensure that the Centerline settings defined in 'File --> Utilities --> Customer Defaults --> Drafting --> General --> Standard --> Customize Standard - Centerline --> General', are used when creating a drafting view with automatic centerlines.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V12.0
Function: ANNOTATION

Ref: 001-7250166

KB Article ID# PL8010637

Contents

SummaryDetails

Associated Components