The font of a custom symbol changes when the symbol is inserted

2019-05-15T15:33:40Z

Summary


Details

The font of a custom symbol changes when the symbol is inserted onto the 
drawing.



Solution

 To retain the same font that the symbol text was created with: 
1. In the Menu, select 'Insert-->Symbol-->Custom'. 
2. In the Setting group of the Custom Symbols dialog, toggle 
 'Annotation Preferences' to 'Use Definition'. 
3. Place the symbol. 
This will use the annotation preferences that the symbol was defined with, 
instead of the current annotation preferences of the drawing.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: KDA
Version: V7.5
Function: REUSE_LIBRARY

Ref: 001-8952651

KB Article ID# PL8010635

Contents

SummaryDetails

Associated Components