Displaying what faces PMI notes are associated in in NX Viewer

2019-08-28T15:00:52Z

Summary


Details

--------------- 
When a part has PMI annotation attached to faces or edges, how can you verify 
what face or edge the annotation is associated to?



Solution

 In NX and NX Viewer, the user can open the Part Navigator and expand PMI. 
Select on the PMI and do a right mouse button and toggle ON the option 
"Associated Objects Mode". This will give a list of associated objects for 
the PMI, for example;


 [-] Associated Object 1 
 [ ] Linear Dimension


 [-] Associated Object 2 
 [ ] Label


 [-] Associated Object 3 
 [ ] Datum Feature Symbol


Selecting on the Associated Object in the navigator will highlight the 
associated faces or edges for the PMI object.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: PMI
Version: V8.5
Function: NOTES

Ref: 001-7604234

KB Article ID# PL8010633

Contents

SummaryDetails

Associated Components