How to split a large Parts List into multiple segments

2019-05-15T15:33:28Z

Summary


Details

If a Parts List is very long, it would be nice to be able to control the length 
of the list, so that after a certain length, a continuation of the Parts List 
is started in a new segment.



Solution

To break the parts list into multiple segments:
 1. Hover the cursor over the top left corner of the Parts List until 
 the entire Parts List is highlighted. 
2. Mouse Button 3-->Settings. 
3 Expand 'Common' and highlight 'Section'. 
4. Set the 'Maximum Height' setting. 
5. Once the Maximum Height has been reached, there is an option to control 
 where the new segment of the Parts List will appear. 
 Toggle the 'Location' setting to 'Left', 'Right', 'Up', 'Down', 
 or 'Next Sheet'. 
6. Close the Settings dialog. 
The Parts List will update as the settings are modified.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V9.0
Function: TABLES

Ref: 001-7351906

KB Article ID# PL8010615

Contents

SummaryDetails

Associated Components