Extruding a Closed Curve Section Does Not Create a Solid Body

2019-05-29T18:45:41Z

Summary


Details

Extruding a closed set of curves results in a sheet body being created rather than a solid body.

Solution

Extruding a non-planer section will result in a Sheet Body being created.  Check to see if the curves in the section are planar.  A couple of quick, simple tests are to see if you can insert a Bounded Plane within the curve section, or Project the curves to a Datum Plane and Extrude them to see if a Solid Body is created.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1847
Function: FEATURE_MODEL

Ref: 001-7192093

KB Article ID# PL8010609

Contents

SummaryDetails

Associated Components