How to remove read-only flag of an orphaned Part Family member?

2019-06-06T15:39:17Z

Summary


Details

--------------- 
You may have the case where you have a large number of part family member parts but for whatever reason do not have access to the Part Family template that created it. These parts are considered to be "orphans" since their parent file is missing. You need to remove the read-only flag from them in order to import these into Teamcenter, but there is no way to remove this flag interactively in NX.



Solution

The NX utility ug_edit_part_names will allow the flag to be removed. To run the utility perform the following steps:


o Launch an NX Command Prompt window 
    Start --> Siemens NX --> NX Command Prompt 
o ug_edit_part_names yourfilename.prt -o yourfilename.prt


The above command will process your file and keep the name the same. When the file is now opened it will no longer be flagged as a Part Family member with a read-only status.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: SYSTEM
Version: V1847
Function: SYSTEM_TOOLS

Ref: 001-7148455

KB Article ID# PL8010606

Contents

SummaryDetails

Associated Components