NX "Additional Model Reference Sets" in customer defaults do not displayed in part.

2019-06-17T12:17:33Z
NX for Design

Summary


Details

--------------- 
Setting "Additional Model Reference Sets" in customer defaults does not create these reference sets in new NX parts.



Solution

These Additional Model Reference Sets are used for generating JT files from the NX parts, not auto-generate reference sets in NX parts.


Documentation/help:


 Data translation -> 
 Writing JT from NX -> 
 Managing the JT output -> 
 Model reference sets:


"Additional model reference sets

If you have additional model reference sets in a single part file, you can 
write multiple, separate JT files for each additional model reference set. You 
can use the Additional Model Reference Sets customer default to define the 
additional model reference sets. If a reference set is not mentioned as the 
Model Reference Set or one of the Additional Model Reference Sets , then a JT 
file is not written for that reference set."





Conclusion: 
--------------- 
No Reference Sets are created due to this default. 
If you need reference sets pre-populated in your NX part files, then add these to your file-new template 
parts.



Notes and References

 
https://docs.plm.automation.siemens.com/tdoc/nx/10.0.3/nx_help/#uid:index_nxtojt:xid504563:xid490362

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: GATEWAY
Version: V10.0.3
Function: CUSTOMER_DEFS

Ref: 001-7700312

KB Article ID# PL8010602

Contents

SummaryDetails

Associated Components

Modeling