Holemaking Drill,Deep,Breakchip parameters/ 840D input fields (CYCLE83)

2019-11-04T08:53:08Z

Summary


Details

Sinumerik 840D


With Deep Hole drilling ( CYCLE83), there is no way in NX of defining:


1) Step depth 
2) Degression factor 
3) Minimum drilling depth



Solution

 This needs to be done with a user defined event 
( There is a discussion about this on our Community website:


https://community.sw.siemens.com/s/question/0D54O000061xPapSAE/cycle83-dam-parameter-negative-value-nx10 )
The solution is to add the definitions into ude.cdl - for example :


PARAM cycle_step_degression_value 

 TYPE d 
 DEFVAL "0.0" 
 UI_LABEL "Value of Degression" 

PARAM cycle_step_degression_percentage 

 TYPE d 
 DEFVAL "0.0" 
 UI_LABEL "Percent of Degression" 

PARAM cycle_step_degression_minimum 

 TYPE d 
 DEFVAL "0.0" 
 UI_LABEL "Minimum Distance" 
}


Add these lines to ude.cdl


EVENT Degression 

 UI_LABEL "Degression"


 PARAM cycle_step_degression_value


 { 
 TYPE d 
 DEFVAL "0.0" 
 UI_LABEL "Value of Degression" 
 } 
}


Then in NX, we get the User defined event - which we can add to the drilling 
op: 
When postprocessing, this shows up as a mom variable in postprocessor


mom_cycle_step_degression_value


The postprocessor would need to be modified the add this into the CYCLE83


( ref ER 8936328 - asking for parameters to be available in NX without need 
for customisation)



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V11.0.1
Function: DRILLING

Ref: 001-8936328

KB Article ID# PL8010601

Contents

SummaryDetails

Associated Components