How do you map to the UGPART-ATTR form in the Named References.

2019-08-28T15:00:14Z

Summary


Details

--------------- 
How do you map to the UGPART-ATTR form in the Named References?



Solution

 1. Export the attribute mapping text file --> open the text file and add the 
 attributes for the UGMASTER dataset as follows; 
------------------------------------------------------------------------------- 
-- 
{ Dataset type="UGMASTER" 
 "DB_PART_NAME" : Item.object_name /write_once /description="Part Name" 
 "DB_PART_DESC" : Item.object_desc /write_once /description="Part 
Description" 
 
 Assembly Number : NR(UGPART-ATTR,UGPartAttr).assemb_no /master=both 
/description="Assembly Number" 
 Creator : NR(UGPART-ATTR,UGPartAttr).creator /master=both 
/description="Creator" 
 Material : NR(UGPART-ATTR,UGPartAttr).material /master=both 
/description="Material" 
 model : NR(UGPART-ATTR,UGPartAttr).model /master=both /description="model" 
 part number : NR(UGPART-ATTR,UGPartAttr).part_no /master=both 
/description="part number" 
 part type : NR(UGPART-ATTR,UGPartAttr).part_type /master=both 
/description="part type" 
 task number : NR(UGPART-ATTR,UGPartAttr).task_no /master=both 
/description="task number" 
 title : NR(UGPART-ATTR,UGPartAttr).title /master=both /description="title" 
 weight: NR(UGPART-ATTR,UGPartAttr).weight /master=both /description="weight"



------------------------------------------------------------------------------- 
-


2. Import the mapping file back into Teamcenter.


3. Start NX/Manager and create a new Item using "Item" as the item type.


4. Go to File --> Properties and enter the values for each of the mapped attributes.


5. Save the part.


6. In Teamcenter, open the Named References for the Ugmaster Dataset --> 
    select the UGPART-ATTR reference --> select Open. In the UGPART-ATTR form you will 
    see the attributes and the values.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V10.0
Function: ATTRIBUTES

Ref: 001-8924376

KB Article ID# PL8010600

Contents

SummaryDetails

Associated Components