How to select all common holes in hole making.

2019-09-04T13:00:20Z

Summary


Details

--------------- 
Does the Hole Making module for drilling offer the 'All Holes on Face' option?



Solution

 No, the Point-to-Point (PTP) module offers the 'All Holes on Face' option but 
Hole Making is a completely different module that utilizes features to machine 
so it does not offer all of the same options. However, the equivalent to that 
option in PTP module would be the grouping of features in Hole Making.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.3
Function: HOLE_BOSS_MILL

Ref: 001-7620837

KB Article ID# PL8010597

Contents

SummaryDetails

Associated Components