Eliminate the pattern feature instances that overhang the body

2019-08-28T15:00:09Z

Summary


Details

--------------- 
Adding a Pattern Feature onto an Elliptical shaped body and there are multiple 
instances that are overhanging the main body. How to eliminate the instances 
that overhang the body?



Solution

 While adding the Pattern Feature, expand the section in the Pattern Feature 
dialog for Boundary Definition. Then set the Boundary option for Face, Curve 
or Extrude. 


In this case the Face option was used and the face that is selected is the 
same face that the Pattern is being applied to. The Curve option could also be 
used and select the outside edge of the face. 


Note: The outside boundary must form a closed loop.


While entering the Pattern direction(s) you will notice that the pattern 
intances will not extend past the edge of the face that was selected for 
the Boundary Condition. You can adjust the Margin Distance to move the Pattern 
Instances to be outside or inside the Boundary if needed.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V8.0
Function: FEATURE_MODEL

Ref: 001-7783244

KB Article ID# PL8010591

Contents

SummaryDetails

Associated Components