How to use the selection filter "Bodies in Group" while creating a Wave Geometry Link?
Solution
1. Define a "Group" in the source part using the command 'Menu -> Format -> Group -> New Group'. This Group must contain one or more bodies.


2. Start the command "Wave Geometry Linker" in the target part and after the dialog pops up, select 'Selection dialog bar -> Selection Intent Rule: Bodies in Group', then select the bodies defined in the Group in the other part file from the graphical window.
Wave Geometry Linker

Bodies in Group

Selecting the bodies that reside in the component within a Group. The quick method is to press the "Select All" button that resides in the Selection Group.

Notes and References
This method applies to all NX releases.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 10_1507
Product: NX
Application: DESIGN
Version: V1855
Function: WAVE
Ref: 001-8818526