NX Edit Parameters not availble from the Part Navigator for Realize Shape

2019-08-28T14:59:48Z
NX for Design

Summary


Details

--------------- 
Edit Parameters is not availble from the Part Navigator for Realize Shape 
features.



Solution

 The user has to select Finish for the current Realize Shape feature then 
select the feature from the Part Navigator and use MB3, the Edit Parameters & 
Edit with Rollback will be available.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: STUDIO_DESIGN
Version: V10.0
Function: SUBDIVISION

Ref: 001-7601702

KB Article ID# PL8010585

Contents

SummaryDetails

Associated Components

Modeling