Needs to suppress trailing zero in X when zero. X0.0 needs to be X0.

2019-07-22T16:49:56Z

Summary


Details

How to get X0. instead of X0.0. when postprocessing.



Solution

In Post Builder under N/C Data Definitions--> Format--> Zero_real, uncheck the 'Output Trailing Zeros' option.  This will give the following output:



N0010 G40 G17 G90 G70 
N0020 G91 G28 Z0. 
N0030 T00 M06 
N0040 G00 G90 X0. Y0. S0 M03 
N0050 G43 Z0. H00 
N0060 Z4.2678 
N0070 X1.1392



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.3
Function: POSTBUILDER

Ref: 001-7634940

KB Article ID# PL8010579

Contents

SummaryDetails

Associated Components