'I-deas ASC/DWG' import function missing from menus

2019-05-15T17:13:56Z

Summary


Details

In the NX Drafting application, under the 'File-->Import' menu, the following 
commands are missing: 
* I-deas ASC/DWG 
* I-deas Symbols


The commands are also not available to be added to a customized toolbar. Why 
are these commands missing from the NX Drafting application?



Solution

 Starting in NX8.0.3, these commands are suppressed if there are no 
DraftingPlus licenses available in the environment.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V8.0.3
Function: INTEROP

Ref: 001-7171440

KB Article ID# PL8010575

Contents

SummaryDetails

Associated Components