How to populate drawing views with a solid with specific features

2019-05-15T15:32:57Z

Summary


Details

How to display a model in a drawing view and show only specific features of the 
model.



Solution

 1. In the Modeling application, with the model as the displayed part, select 
 in the Menu, 'Insert-->Associative Copy-->Extract Geometry'. 
2. Set Type to 'Body'. 
3. In the Settings grouping, toggle on 'Fix at Current Timestamp'. 
 This will create an associative copy of the solid with only the features 
 created before the current Timestamp. 
4. In the Menu, select 'Format-->Move to Layer'. 
5. Select the extracted body. 
6. OK the dialog. 
7. Specify a unique layer for the extracted body. 
8. [Optional] If needed, repeat steps 1-8 to create an extracted body 
 for each set of features to display in a drawing view. 
9. Switch to the Drafting application with the drawing as the displayed part. 
10. Place a view on the drawing. 
11. In the Menu, select 'Format-->Layer Visible In View'. 
12. Make the layer visible that contains the extracted body with the 
 desired features to be displayed. 
13. Make all other layers Invisible.


This technique can be used to show the same solid in various stages of 
development in separate drawing views.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V9.0
Function: DRAWING/VIEW

Ref: 001-8946771

KB Article ID# PL8010569

Contents

SummaryDetails

Associated Components