Initial secondary number is not in valid format when reset drafting preferences

2019-05-21T20:42:29Z

Summary


Details

Perform Drafting Preferences reset by Loading from Setting Source = Customer Defaults, it is failing with following error:


The initial secondary number is not in valid format



Solution

In Drafting standard, the default value defined for Drawing Sheet format, there is a required condition in NX that may trigger such an error:


If the primary character is a numeral, then the secondary character must be a letter. Likewise a primary letter character requires that the secondary character be a numeral.


Examine the settings in your Customer Defaults:


For NX8.5 and NX9: 
Drafting -> Drawing, General tab: 

Make sure Initial Sheet Number and Secondary Number are not both numeral or both letter.



For NX10: 
Drafting Standards -> Drawing Format -> Sheet, in the "Name and Number" tab: 

Make sure Initial Sheet Number and Secondary Number are not both numeral or both letter.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V11.0
Function: ANNOTATION

Ref: 001-7572604

KB Article ID# PL8010564

Contents

SummaryDetails

Associated Components