How can I track the center of a Ball mill in a Blade Finish operation?
Solution
When postprocessing the toolpath...select "Output Ball Center".

"
Output Ball Center" triggers the MOM_ball_center_output event before the MOM_start_of_path event for all operations in which the tool is a mill tool and the tool subtype is one of the following: SPHERICAL_MILL BALL_MILL MILL with Diameter =Lower Radius * 2
You must add the enable_ball_center_output to your postprocessor. For more information, see
Enable center of ball output.
Notes and References
For more information, see Enable center of ball output. https://docs.plm.automation.siemens.com/tdoc/nx/1872/nx_help/#uid:xid923170Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1872
Function: MULTI_BLADE
Ref: 001-7565188