Can't select geometry from multiple drawing views to create a custom symbol

2019-05-15T15:32:46Z

Summary


Details

Geometry from multiple drawing views is not selectable when creating a custom 
symbol.


By design, the custom symbol creation code does not allow selection of geometry 
from multiple drawing views.



Solution

 To create a custom symbol that consist of geometry from multiple drawing views, 
perform the following: 
1. With the drawing open, select 'File-->Export-->CGM'. 
2. On the Export CGM dialog, under the Source header, select the sheet 
 or 'Current Display', to include the contents needed for the symbol. 
3. Specify a Destination folder. 
4. Set Properties and Settings options as needed. 
5. OK the Export CGM dialog. 
6. In the NX, go to the Drafting application. 
7. Create a new blank drawing sheet by selecting 'Insert-->Sheet'. 
 Select an appropriate standard size and units. 
8. OK the Sheet dialog. 
9. After confirming the new blank sheet is active, select 
 'File-->Import-->CGM'. 
10. Browse and select the CGM file created in steps 1-5. 
11. OK the Import CGM File dialog. 
12. The geometry from multiple views in the CGM will be imported to the blank 
sheet. This imported geometry can be selected for creating a custom symbol.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V7.5
Function: SYMBOL

Ref: 001-6907708

KB Article ID# PL8010558

Contents

SummaryDetails

Associated Components