How do you create the Radius to Center dimension style?

2019-06-07T14:19:07Z

Summary


Details

How do you create the Radius to Center dimension style?

Solution

 To create the Radius to Center dimension style like prior to NX9, you have to use  Radial icon on the ribbon toolbar --> Set the method to Radial --> Select the circle/arc to dimension in the graphics window --> MB3 -> You would get Radius to Center.


Note: If you use the Rapid dimension, you can also access Radial dimension and get the same result.




Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V12.0.2
Function: DIMENSION

Ref: 001-7273546

KB Article ID# PL8010551

Contents

SummaryDetails

Associated Components