NX Vericut - NX 10.0 Interface - Procedure entry point error

2019-11-01T13:39:41Z
NX for Manufacturing

Summary


Details

When launching NX 10.0 with the Vericut interface (10.0 & 10.0.1)


Gives following warning window: 
The procedure entry point UF_UI_ONT_ask_selected_nodes could not be located in the dynamic link library libugopeniny.dll. 
After a click on OK, NX seems to open ok.


(Not a problem with NX 9.0)



Solution



CGTech are aware of a problem with V7.3.4 starting NX10.0 via the VERICUT NX 
batch file.


Interface is supplied by CGTech, and updates are available from following:


CGTech Support: http://www.cgtech.com/vericut_support/


USA Contact:
Tel.: (949) 753-1050
Email: support@cgtech.com


UK Contact:
CGTech Ltd
Curtis House, 34 Third Avenue, Hove, BN3 2PD
Registered in England No: 3579362 VAT No: 717604145
 
Tel: +44 (0) 1273 222908
Email: support.uk@cgtech.com



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.1
Function: VERIFY

Ref: 001-7346941

KB Article ID# PL8010538

Contents

SummaryDetails

Associated Components

Manufacturing General