Fillet Welds do not have a Weld Class, but Spot welds do

2019-08-28T15:00:19Z

Summary


Details

--------------- 
In Weld Assistant, the Spot weld option has a Weld Class but the Fillet Welds 
do not. How can you add the weld class for Fillet Welds?



Solution

 In the Customer Defaults for Weld Assistant. Go to "Creation" and first select 
the "Resistant Spot" weld tab and notice in the Characteristics it has a list 
for WELD_CLASS. 


 List:Class:WELD_CLASS:I,II,III:III:::Required


Copy and Paste that line into the Characteristics for Fillet Weld. Restart NX 
and open your part and add a Fillet Weld, but before Applying the weld go into 
the Welding Characteristics section of the dialog and you will now have an 
option now for "Class", if you select the cell in the Value column it will 
have a drop down to set it to either I, II, III, User Defined...



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: KDA
Version: V9.0
Function: WELD_ASSISTANT

Ref: 001-7565178

KB Article ID# PL8010528

Contents

SummaryDetails

Associated Components