Simcenter 3D Solutions Thermal load with heater controller not working.

2020-11-10T20:48:57Z
Simcenter 3D

Summary


Details

I have a proportional heater controller setup in my model and the load will 

not activate, even when the sensor element is well below the cut-in 

temperature. Why is this happening?

Solution

The single most common cause for problems with heater controllers not 

functioning as expected is failing to set the solution to one of the advanced 

solution types(advanced thermal, advanced thermal-flow, NX advanced 

Thermal/Flow with ESC). The use of an advanced license is required to use a 

heater controller. If the solution is not set to one of the advanced 

solutions, then the load with a heater controller will not be written out. The 

only indication of this is a warning, similar to the following, in the 

solution export log:

Modeling Object Error Summary 

=============================

WARNING

Active Heater Controller = Active Heater Controller1 

Unsupported entity will be ignored for this solution.

Note that the advanced solution types do require an additional license. If the 

user does not have an advanced thermal license, the solution will fail with 

licensing error. 

The following document discusses the differences between the standard and 

advanced solution types and will list what features require an advanced 

license. 

https://docs.plm.automation.siemens.com/tdoc/nx/10.0.3/nx_help/#uid:id1375637

Notes

KB Article ID# PL8010503

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow