Why the part location is different in wireframe mode than in shaded mode.

2019-06-07T14:18:49Z

Summary


Details

If the facet is corrupted in the part file, then the shaded display part is 
located at a different location than in wireframe mode.
How can you fix this problem?



Solution

 Because the facet of the part was corrupted and saved in the part, you have to 
recreate the new facet using the method below: 
Go to Menu --> Preferences --> Visualization Performance --> General Graphics tab --> 
 Under Part Settings --> Toggle off Save Shaded Display Facets --> Save the part --> 
 Reopen it --> Then you can toggle it back on --> Save the part for NX to recreate the facet. 




Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V12.0.2
Function: VISUALIZATION

Ref: 001-7926820

KB Article ID# PL8010501

Contents

SummaryDetails

Associated Components