Process Secondary Geometry is off but Secondary Components list exist

2019-05-15T17:12:42Z

Summary


Details

Creating a view in the Drafting application results in this message: 
 Process Secondary Geometry is off but Secondary Components list exist.



Solution

 Check to see if any of the drawing components are designated as "Secondary 
Geometry". 
1. Hover the cursor over the component in the Assembly Navigator, 
 'MousButton3-->Properties'. 
2. Select the 'Drawings' tab. 
3. Check to see if 'Secondary Geometry' is toggled ON. 
 Check this for all components.


Option A: 
If component(s) are not to be 'Secondary Geometry', simply toggle this option 
off. 
Option B: If the components need to remain 'Secondary Geometry', then process 
the Secondary Geometry in the drawing. 
1. In the Menu, select 'Preferences-->Drafting'. 
2. Expand 'View-->Common' and highlight 'Secondary Geometry'. 
3. Toggle ON the Process of 'Secondary Geometry'. 
4. OK the Drafting Preferences dialog.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V11.0
Function: DRAWING/VIEW

Ref: 001-7882381

KB Article ID# PL8010488

Contents

SummaryDetails

Associated Components