Unable to explode WAVE geometry in an assembly

2019-05-15T17:15:07Z

Summary


Details

Why is the WAVE linked geometry in an assembly unable to be exploded?



Solution

 The WAVE geometry needs to be made position independent into order for it to be 
moved independently or exploded. However, when an 'Edit Parameters' is 
performed on a WAVE Linked Body, the 'Make Position Independent' option is 
missing from the WAVE Geometry Linker dialog. 


A WAVE license is needed for the 'Make Position Independent' option to appear 
in the dialog.


To determine if a WAVE license is available: 
1. In the Assembly Navigator, hover the cursor over one of the column headers. 
2. 'MouseButton3-->WAVE Mode'. 
If 'WAVE Mode' turns ON successfully, a WAVE license can be obtained. 
However, if the following message is received, a WAVE license is not available: 
 Unable to obtain a WAVE Control license.


If a WAVE license is not available, this could be the reason why the 'Make 
Position Independent' option does not appear in the WAVE Geometry Linker 
dialog.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V7.5
Function: WAVE

Ref: 001-6834335

KB Article ID# PL8010484

Contents

SummaryDetails

Associated Components