Customer would like to see the G90 code output before the G43 code on the same line of code.
Solution
By default, G43 is output before G90, but this can be changed. Take a look at the master list for output order inside of postbuilder under Program & Toolpath--> Word Sequencing.
Find the G90 block here and drag it into place somewhere before the G43 block. This globally changes the order in which these words are output. If you now go back to the rapid move event where these codes are coming from, you should see the order on that line is now changed.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.3
Function: POSTBUILDER
Ref: 001-7436954