Set U and V on Circular Planar Surface to be Concentric and Radial.

2019-05-02T12:44:38Z

Summary


Details

How to make a U and V grid concentric circles and radial spokes versus perpendicular lines on a circular surface?



Solution

Use the function "N-Sided Surface" and change the Type from Trimmed to Triangular. This will change the U and V orientation control from perpendicular lines to circular lines with radial spokes coming from a central point on the surface.


The Shape Control section in the dialog allows adjusting the center-point location between the perimeter in all directions.

Steps on how to set the U and V grid lines on a circular surface.

1. The circular face.

2. N-Sided Surface selection.

3. Set N-Sided Surface to Triangular.

4. Select the outer edge of the surface.

5.  Select OK once the edge has been selected.

6a. Change the shaded display to Wireframe - Classic method of pressing the third mouse button (opposite button on the mouse that you press to select objects).

6b. Change the shaded display to Wireframe - Icon method.

7. Select the function "Edit Object Display".



8. Select the N-Sided circular surface.

9. Select OK on the dialog to accept.

10. Under the "General" tab, expand the option group "Wireframe Display".

11. Select and change the zero (0) values for U and V to some value.  Inserting five (5) for this example (see the blue box below).

12. Here is the final result with a U and V setting value of five (5).


Notes and References

Applies to all NX releases that have the N-Sided Surface function available.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 10_1507
Product: NX
Application: DESIGN
Version: V1847
Function: FREE_FORM_MODEL

Ref: 001-8821945

KB Article ID# PL8010471

Contents

SummaryDetails

Associated Components