The Offset command in Sketcher has a 200 segment limitation

2019-05-15T15:32:01Z

Summary


Details


When using the Offset command in a Sketch to offset curves, only 200 curve 
segments can be selected at one time.



Solution

  This is As Designed.
The 200 curve segment limitation is there to prevent a performance issue. 
Offset is typically a complex constraint. 
So a restriction of 200 curves when creating an Offset was established, as that would result in at least 400 constrained curves (200 base and 200 outputs).



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V5.0
Function: SKETCHER

Ref: 001-6838833

KB Article ID# PL8010469

Contents

SummaryDetails

Associated Components