Copy faces of a solid body as sheets to another part file

2019-06-04T16:58:26Z

Summary


Details

--------------- 
How can you copy a set of faces from a solid body in one partfile to another 
and not the associated objects?



Solution

 In the original part file, select Edit --> Feature --> Remove Parameters --> 
select the solid body(s) and OK.


File --> Export --> Part --> select Existing Part and press the Specify Part 
button. Select the part to export to --> OK. Select the Class Selection 
button and select the faces --> OK --> OK.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V1867
Function: FEATURE_MODEL

Ref: 001-6839780

KB Article ID# PL8010461

Contents

SummaryDetails

Associated Components