Setting up an Effectivity Occurrence rule

2019-06-06T20:39:04Z

Summary


Details

--------------- 
How can you set up an Effectivity Rule in Structure Manager to open a specific 
component in NX?



Solution

 1. Using an assembly with two similar items (two different configurations of 
the same component), you want to use the older version (based on the Last 
Modified date of the file) up to a certain date. After that date, you want to 
use the newer version.


2. In the assembly, make the component the work part and perform a Save As New 
Item on the component. This creates the newer version of the component. Add 
the older version back into the assembly and Save/Close.


3. In Teamcenter, send the assembly to the Structure Manager. Under the 
Occurrence Effectivity ID column, double-click the row under this column that 
contains the older component. You will see a Occurrence Effectivity dialog 
open.


4. Enter the rule name in the Occurrence Effectivity ID field. Then set the 
From and To dates that the rule will apply. Do the same for the newer 
component. Again, the rule will apply to the Last Modified date of the 
partfile. Save the assembly.


5. Selecting View --> Show Unconfigured by Effectivity Occurrence toggle to on 
will show the assembly structure how it will load today. The invalid 
component will not be listed.


6. In NX, the assembly will load based on the rule. You will not see the 
suppressed component unless you toggle on Include Suppressed Components in the 
Assembly Navigator. The component will be listed in the navigator with a blue 
box icon and a dashed box. You cannot unsuppress the component. You would 
need to change the rule in the Structure Manager.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1876
Function: FILE_OPEN

Ref: 001-6565849

KB Article ID# PL8010459

Contents

SummaryDetails

Associated Components