---------------
What is the operation subtype limit on the dialog and the row/column limits?
Solution
Currently the number of subtypes per row have a maximum of 6. There is no limit on the number of subtypes that can be added to a CAM template dialog.
A slide bar on the right hand side of the dialog will become available when the dialog becomes too tall.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: CAM
Version: P1859
Function: TEMPLATES
Ref: 001-7678791