---------------
While editing a routing spline path and selecting on a spline point, the
dynamic CSYS is displayed. How can you change the direction of the vectors
other than using the drag handle to Rotate?
Solution
Select the Arrow Head on the dynamic CSYS. Then use MB3 and select
Specify Direction. This will Open the Vector dialog to specify the vector
direction.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ROUTING_GENERAL
Version: V8.5
Function: PATH
Ref: 001-7410558