NX Editing the distance of Sketch Offset Curve when no dimension is shown.

2019-06-04T18:52:15Z
NX for Design

Summary


Details

---------------
When working in Sketcher and creating an Offset Curve, you enter a value in the "Distance" field and the "Create Dimension" toggle is off. You later go and edit the Offset Curve by double clicking the Offset constraint in the sketch but the dialog does not display the Distance field. How do you edit the distance?



Solution

The logic used in the Offset Curve dialog is that when the user creates a dimensionless offset ("Create Dimension" unchecked), the user will use some other constraint or dimension to drive the offset constraint distance. Therefor we do not allow it to be driven by an offset dimension automatically, unless the user asks for it.



You may edit the existing Offset Curve in the sketch by toggling "Create Dimension" on to display the "Distance" field again. Leaving the "Create Dimension" toggle on will create a "Thickness Dimension" on the sketch, which when edited will bring the user directly to the "Distance" field in the Offset Curve dialog.





Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: DESIGN
Version: V1847
Function: SKETCHER

Ref: 001-7269398

KB Article ID# PL8010451

Contents

SummaryDetails

Associated Components

Modeling