How to delete a lightweight body without deleting the parent solid body

2019-05-15T15:31:50Z

Summary


Details

Deleting a lightweight body is deleting the parent solid body. 
How can the lightweight body be deleted without deleting the parent solid body?



Solution

 1. Make sure 'History Mode' is being used. 
 Select 'Insert-->Synchronous Modeling-->History Mode'. 
2. Make sure 'Timestamp Order' is turned off. 
 In the Part Navigator, place the cursor over one of the column  headers, 'MB3-->Timestamp Order'. 
3. In the Part Navigator, the lightweight body will show up as a dependent 
 of the solid body and can be selected for deletion.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V7.5
Function: PART_NAVIGATOR

Ref: 001-7185773

KB Article ID# PL8010450

Contents

SummaryDetails

Associated Components