Lock the CALLOUT attribute at the Component level

2019-05-15T17:10:08Z

Summary


Details

Component Properties allows the CALLOUT attribute to be modified at both the 
'Instance' level and the 'Component' level. Situations where the CALLOUT 
attribute has a different value at the 'Component' level vs. the 'Instance' 
level can cause confusion. 
How can the CALLOUT attribute be locked at the 'Component' level so it cannot 
be modified and will always have the same value as the 'Instance' level?



Solution

 Starting in NX10, there is a Customer Default that controls this: 
1. Select 'File-->Utilities-->Customer Defaults'. 
2. Expand 'Assemblies' and highlight 'General'. 
3. Select the 'Instance Attributes' tab. 
4. Toggle OFF 'Allow CALLOUT Attribute Override'. 
5. OK the Customer Defaults dialog. 
6. Re-start NX. 
Now on the Component Properties dialog ('Attribute' tab), if the Context is 
set to 'Component', the CALLOUT attribute is locked and cannot be modified. 
However if the Context is set to 'Instance', the CALLOUT attribute is still 
modifiable.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V10.0
Function: ATTRIBUTES

Ref: 001-7961096

KB Article ID# PL8010449

Contents

SummaryDetails

Associated Components