"No Write permissions at the input directory" exporting DXF file

2019-08-12T13:25:11Z

Summary


Details

When trying to to Export a DXF File from NX, "File-> Export-> DXF", the following error is displayed, 


 "No write permissions at input directory, 
 Saving the part file at ..."


 <OK>



Solution

Investigating further, the following error can be found in the NX SYSLOG file, (File-> Help-> Log File);


 +++ The customer default used an invalid font name, Arial Unicode MS 


The FONT name may be different, but the error indicates that a particular Font is missing from your system. To verify that the font is/is not installed, click Start, and in the 'Search programs and files' window, type the following command, and then press the Enter key:


 %windir%\fonts


If you see the 'missing' from the error message above, right-click on the font and select 'Install'. 


If the font is not listed, and it is a standard Windows font, run Windows Setup again. Setup replaces missing or changed files. If the standard fonts are missing, other Windows files may also be missing. Setup also reinstalls these files.


Warning If you run Windows Setup, you may lose programs and hardware drivers that you have installed since the last time Windows was set up on your computer. 


The following fonts are included with Windows and are installed on every 
computer: 


 o Courier New (TrueType, including Bold, Italic, and Bold Italic variations) 
 o Arial (TrueType, including Bold, Italic, and Bold Italic variations) 
 o Times New Roman (TrueType, including Bold, Italic, and Bold Italic 
 variations) 
 o Symbol (TrueType) 
 o Wingdings (TrueType) 
 o MS Serif 
 o MS Sans Serif



Notes and References

Problem Report #7277264



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: SYSTEM
Version: V1867
Function: WNT_OS_ISSUES

Ref: 001-7441968

KB Article ID# PL8010445

Contents

SummaryDetails

Associated Components