NX NX Load options are different when opening an assembly from TC.

2019-06-07T14:18:45Z
NX for Design

Summary


Details

--------------- 
When you open an assembly from TC by selecting the item revision, then select 
the NX icon to open, the NX load options might be different than if you launch 
NX first then do File --> Open. Why and how do you fix it?



Solution

 When you launch NX first in TC portal, then go to File --> Assembly Load Options, you can set NX load options here before you open the assembly and you can save the load options to a load_options.def file. 


However, when you load the assembly from TC by selecting the item revision 
and launch NX, the load options might be different. What controls load options 
in this case?


In TC, there is a preference could override NX load options:


TC_NX_Navigator_Override_NX_Load_Option


Valid Values 
As Saved - Loads the part file as it was saved in Teamcenter Integration for NX.


Latest - Loads the part file with the latest revision rule.


None - Ignores the As Saved command and loads the assembly as defined in 
load_options.def file. 


Default Values: Latest



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_OPEN

Ref: 001-7108711

KB Article ID# PL8010432

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX