NX FCC_RollbackFileUploadedToPLM Invalid ticket or pointer on save

2019-10-04T07:43:33Z
NX for Design

Summary


Details


When saving a routing assembly there is an Error message: 


"Error detected during FMS operation"


"The function FCC_RollbackFileUploadedToPLM() returned the following status: 
Please see your system administrator for assistance. Invalid ticket or invalid ticket pointer."



Solution

 Turn off the option "Publish the chosen feature categories to Teamcenter" for "routing data", in the customer defaults.


File --> Utilities --> Customer defaults --> Teamcenter Integration for NX --> General --> tab: Feature --> And uncheck here: Routing Data.


The information published to Teamcenter needs more configuration. In most cases this is not needed or used and this setting should remain unset.



Notes and References

IR/PR 1968013 
IR/PR 1901778 
IR/PR 1857098



Hardware/Software Configuration

Platform: all
OS: window
OS Version: ALL
Product: NX
Application: ROUTING_GENERAL
Version: V12.0
Function: PREFERENCES

Ref: 001-1968013

KB Article ID# PL8010415

Contents

SummaryDetails

Associated Components

Routing