Details
When attempting to use an end mill with a Rotary Floor operation, the message "only ball nose end mills are supported" is given.
Solution
There is confusion caused by using the term "end mill", the correct term is "ball mill" (as shown on the tool definition)
a spherical mill is also a valid tool:
see PR 8850257 requesting change of message to:
"only ball mill and spherical mill tools are supported"
Notes and References
PR 8850257
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V11.0.1
Function: MILLING
Ref: 001-8850257