WAVE-linked parts loaded after saving of component

2019-05-08T09:46:15Z

Summary


Details

--------------- 
PROBLEM DESCRIPTION 
=================== 
If a component has WAVE-linked geometry from other components we get the 
following trouble: 
After saving the component all parent components of WAVE-linked geometry are 
automatically loaded. 
If we have a lot of such parent components NX hangs.


STEPS TO REPRODUCE
==================
- open TC
- create assembly of 3 components (part1, part2, part3)
- create solid bodies in part1 and part2
- make part3 "work part"
- run "Wave Geometry Linker" and link solid bodies from part1 and part2
- "Force save all"
- close all parts
- go to "My Teamcenter" and open in NX only part3
- save
- look at "Window\More" and note: all WAVE-link parrents are loaded.

For NX12: Window\Change Displayed Part



Solution

 SOLUTION 
======== 
In NX: 
Go to: File\Utilities\Customer defaults\Teamcenter Integration for NX\Feature.


- remove flag on "Spot Weld"
- remove flag "Legacy" on "Weld Publishing Method"

Combination of these flags get this effect.


It's connected with storage type of Weld Points in Teamcenter.


(More details about this method see in Documentation: "Teamcenter Integration 
for NX\Advanced management of data\Weld and Datum Point Publishing")


Upload of WAVE-link parents during saving doesn't depend on presence/absence 
of Weld Points in components. 
It happens even there are no Weld Points in the assembly at all.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 2012
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: ASSEMBLY

Ref: 001-8279036

KB Article ID# PL8010402

Contents

SummaryDetails

Associated Components