A
Postprocessor Error message is displayed when opening an operation in
NX.
After this message is displayed and when attempting to edit the
Start of Path or
End of Path Events the
Events Available menu is empty.
In some earlier versions of
NX this menu might only show a limited set of
User Defined Events (UDE). What could be causing these display issues?
Solution
If edits were made to the
ude.cdl and the syntax of one of the commands was made incorrectly then display issues will result. Rename the edited
ude.cdl and restore the out of the box version. Add each custom
UDE back in one at a time and test it until the problem
UDE is identified.
Be sure and check the very last line of the
ude.cdl file. Entering either a blank line or a "}" character will work. Notice below that using the "#" character will cause a failure.
This will work:
This will work:
This will not work:
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1859
Function: USER_DEF_EVENT
Ref: 001-7492737