How to add additional text to a Hole Callout

2019-05-15T15:31:38Z

Summary


Details

How to add additional text to a Hole Callout.



Solution

 1. Before placing the Hole Callout, select the 'Settings' icon on the dialog. 
2. In the Settings dialog, select 'Prefix/Suffix'. 
3. Select the Parameter drop-down menu to toggle 'Depth' or 'Diameter'. 
 For example, for 'Depth', the default Prefix is a "-", and the 
 Suffix is "DEEP". 
 NOTE: Additional text can be entered for either field. 
4. OK the Settings dialog. 
The new text will be displayed when the Hole Callout is placed.


To set this as a Drafting Preference: 
1. Select 'Preferences-->Drafting'. 
2. Expand 'Common' and highlight 'Prefix/Suffix'. 
3. Scroll down to the 'Hole Callout' grouping. 
4. Set the Feature appropriately and select the Parameter to add text. 
5. Modify the Prefix and Suffix as desired. 
6. OK the Drafting Preferences dialog. 
Any new Hole Callouts will have the modified Prefix/Suffix.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V10.0
Function: DIMENSION

Ref: 001-7808929

KB Article ID# PL8010399

Contents

SummaryDetails

Associated Components