Manufacturing tutorials do not open correctly.

2019-05-15T15:31:21Z

Summary


Details

User is trying to launch an NX manufacturing tutorial. The html document pops 
up correctly, but the system opens a new NX session with no parts in it rather 
than opening the parts for the tutorial in the current NX session.



Solution

This is because the .pax file type for the tutorials has been associated with 
the main NX program. These should be associated to the "NX Component" 
program. This is a windows setting, not NX. To resolve this: 


 - Shut down all NX sessions. 
 - Go into: 
 Control Panel 
 Programs 
 Make a file type always open in a specific program


 - Find the .pax file type in the list and select it. 
 - Pick the Change Program button. 
 - Expand the 'Other Programs' section of the dialog. 
 - Pick the "NX Component" program from the list.


Note: You will have to have administrator permissions on the computer to see 
this program in the list of available choices.


 - Restart NX and verify that the tutorials function correctly.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: CAM
Version: V10.0.2
Function: DOCUMENTATION

Ref: 001-7556290

KB Article ID# PL8010391

Contents

SummaryDetails

Associated Components