How to project a decal or a curve onto a surface without distortion

2019-05-15T15:31:13Z

Summary


Details

How to project a decal or a curve onto a surface without distortion. 
This will ensure the arc length of the projected curve is the same as the arc 
length of the original curve.



Solution

 1. Select 'Insert-->Curves-->Curves From Curves-->Project'. 
2. Expand the Projection Direction group in the dialog. 
3. Set 'Direction' to 'Along Vector'. 
4. Select a vector arrow from the work area. 
 NOTE: Select 'Reverse Direction' if needed to get the vector to point 
 to the curved surface. 
5. Set 'Project Option' to 'Equal Arc Length'. 
6. Select a point on the original curve to 'Specify XY Origin'. 
7. Select a vector arrow from the work area to 'Specify X Direction'. 
8. Under the Curves or Points to Project group, select the original 
 curves for projection. 
9. Under the Objects to Project To group, select the face to project onto. 
10. OK the Project Curve dialog.


The arc lengths can be confirmed by using 'Analysis-->Measure Length' and 
selecting the original and the projected curve(s) for comparison.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V8.5
Function: CURVE

Ref: 001-7178324

KB Article ID# PL8010387

Contents

SummaryDetails

Associated Components