---------------
Feature Based Machining finds the oval pocket but fails to add the geometry to
the Planar Mill operation.
Solution
In a case like this you need to highlight the feature and perform a 'Create
Feature Process' to see what type of operation that the feature rules are using
to machine the oval pocket. In this case, we found that a Cavity Mill
operation was the operation of choice and all the geometry was added to the
operation.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.3
Function: FEATURE_BASED
Ref: 001-7785987