---------------
When adding a Hole Callout dimension, they do not have filled Arrowheads.
Editing the template part files, ansi.atp.prt, iso_din.atp.prt, etc. the
Settings dialog does not have the option for arrowhead type. How do
you change the template so that the dimensions have Filled Arrowheads?
Solution
In NX9, the Radial Dimension Measurement Method for Hole Callout replaced the
Feature Parameters command. The Hole Callout dimensions are now created per
the current Drafting Standard settings.
But, when adding a Hole Callout from the Radial Dimension dialog, the user
does have full control of the dimension style. At the bottom of the dialog
is the Settings section and it contains the Settings icon or while dragging
the dimension use MB3 --> Settings, where the user can change the Arrowhead
type to Filled Arrow, and other style settings.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V9.0
Function: ANNOTATION
Ref: 001-7964105